Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a lug that will accept 4-3/0 conductors per phase on a PGA36080?
Issue:
Lugs for a P-frame I-line breaker that accept four (4) 3/0 cables per phase

Product Line:
Molded Case Breakers

Environment:
Powerpact P

Cause:
Installation

Resolution:
An AL1200P24K will accept 4-3/0 to 500 kcmil per phase.
AL1200P24K has 1 lug per kit.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings