Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the 1000 A EZM main, EZM31000CB, be converted in the field to a 1200 A EZM main, EZM31200CB?
Issue:
Product design features

Product Line:
EZM metering

Resolution:
No. The wiring diagram of an EZM31000CB limits the ampere rating of this device to 1000 A maximum.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings