Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Model 6 Motor Control Center Cover Screws
Issue:
What is the part number for the 10/32 x 1.25" hex head screws for the covers on a Model 6 motor control center?

Product Line:
Model 6 motor control centers

Environment:
Maintenance/replacement/repair

Cause:
Relacement of lost, damaged cover mounting screws

Resolution:
The catalog number for the 10/32 x 1.25" hex head screw is 80450-227-01.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings