Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a field installable shunt trip kit for EDB, EGB, or EJB breakers?
Issue:
Can a shunt trip accessory be field installed on an E frame circuit breaker? (EDB, EGB, EJB)

Product Line:
E frame breakers for NF panelboards

Resolution:
The electrical accessories for E-frame breakers are factory-installed only.
  • Auxiliary Switch/ Alarm Switch (AABA Suffix)
  • Shunt Trip (SA Suffix)
  • Auxiliary Switch/ Alarm Switch/ Shunt Trip (AABASA Suffix)
  • Alarm Switch for EPD ONLY (BA Suffix)
Note: Accessories add an additional pole space to the breaker.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings