Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What circuit breaker type is used in PFA, PKA, PBLA, and PTMA busway plug-in units?

CORRECTION: The Legacy circuit breaker line for busway plugs is now obsolete.  These have been replaced by the Powerpact line of circuit breakers, selection based on SCCR and trip unit required.  Refer to the current online Digest for a selection of these devices.  Note that the Powerpacts will NOT retrofit into the old plug; the entire plug has to be changed out.

Issue:
Circuit Breaker used in PFA, PKA, PBLA, and PTMA busway plug-in units

Product Line:
I Line Busway, busplugs

Environment:
Replacement breakers for busplugs

Cause:
The intermittent tripping issues and worn parts

Resolution:

FAP for PFA plug-in unit
KAP for PKA plug-in unit
LAP for PBLA plug-in unit
MAP for PTMA plug-in unit

The KAP and MAP breakers above are obsolete and no longer available.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings