Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an HU364, series E1 (or E01) heavy duty safety switch?
Issue:
Obsolete design repair parts

Product Line:
Safety Switches

Resolution:
The parts listed here are the only field replaceable parts that are still available.
Lug assembly - 4025116251 (6 required)
Line base phase insulator - 4052025301 (2 required)
Dust shield - 4051136201
Line and load base mounting screws - 4020506501 (2 required per base)
Handle knob kit - 4028344050K

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings