Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the short circuit rating of a size one starter at 480V with HJ and HL breakers?
Issue:
SSCR for starter Size 1 at 480v using HJ/HL Breakers

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
HJ-HL breakers

Resolution:
Model 6 size 1 Nema type ``S`` starter units with circuit breaker disconnect 480V with HJ mag guard is 65KA. HL mag guard is 100KA. With HJ thermal mag is 65KA and an HL thermal mag is 100KA.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings