Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What hubs can be used with EZM Mains to enter the enclosure through the top endwalls of combination overhead/underground units?
Issue:
Product Design Features

Product Line:
Metering Equipment

Resolution:
EZM Main Circuit Breakers, Main Fusible Switches and Main Lug Tap Boxes are all supplied with solid Top Endwall / Driphoods without provisions for gasketless hubs and without knockouts. For cable and conduit through the Top Endwall of these EZM Mains will require that hole(s) be cut through the Drip hood and if installed outdoors UL Listed Liquid-Tight or Water-Tight Hubs must be used. Example of Hubs with gaskets suitable for use here include: B300, B350, B400, H100, H200, H300 & H400. NOTE: Do not use gasketless hubs that require an endwall with a special lip pattern pre-formed in the endwall. Examples of gasketless hubs not suitable for use outdoors with these mains include: B-250, A-200 or A300L.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings