Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How is the EHB breaker removed from a NEHB panel?
Issue:
How is the EHB breaker removed from a NEHB panel?

Product Line:
NEHB Panelboard, EHB Breakers

Resolution:
  1. First make sure power to the panel is off and that the bus is not live.
  2. Pull the outside edge of the breaker towards you so that it comes off the mounting rail.
  3. Pull the breaker towards the wire gutter. The flexible connector will unfold and expose the screw head of the bolt.
  4. Unscrew the bolt connecting breaker to the panel.
Both NEHB panelboards and EHB breakers are obsolete. All parts and accessories are not available.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings