Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does the QO/QOB molded case switch have a magnetic trip?
Issue:
Can a molded case switch trip?

Product Line:
Miniature Circuit Breakers

Resolution:
No, it is a non-automatic switch that provides no means of tripping. The QOB200 is a 2 pole, non-automatic molded case switch and is limited to 60 A max in operation. It has no circuit protection capabilities and is for switching circuits on or off only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings