Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the shelf life for the 9012 type G pressure switches?
The shelf life is dependent on the diaghragm. Ambient conditions may affect the life span adversely, especially if subjected to high or low temperatures or humidity levels.

Buna-N (nitrile) is 2 to 5 years.
Vtion is up to 20 years.
Ethylene Propelene is up to 10 years.


CTA-ID : 2053860

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings