Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is factory installed bus or conductors provided for the second field installed service disconnect on ALL the 400 A CSEDs?
Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Resolution:
The appropriate bus or conductors that would be required from the load side of the meter socket to either the service disconnect base or factory installed lugs will be factory installed. Depending on the exact design layout of the 400 A CSED, it might require the installer to field install conductors from the lugs or base to the disconnect once it is field installed.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings