Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are integral TVSS products available for the EZM metering?

Article available in these languages: Spanish

Issue:
Product availability

Product Line:
EZM Metering equipment

Resolution:
The below New catalog SPD numbers along with the mounting kit MMSAMK400 can be field installed inside EZM main devices. See the attached instruction bulletin for the mounting kit

ApplicationObsolete Catalog #New Catalog number
120/240 Vac Single Phase420120SP05AWSJ10SPDE1
208Y/120Vac  3phase420120YP05AWSJ10SPDE2
240/120 Vac High Leg Delta420240HP05AWSJ10SPDE3A
240 Vac 3phase Delta420240DP05AWSJ10SPDE6A


NOTE: The horizontal cross bus in EZM main devices has been drilled and tapped to accommodate the screws and ring terminals provided in the MMSAMK400 mounting kit. The MMSAMK400 is NOT configured for use inside an EZM branch unit.

Another potential option would be to use an EMA surge device, which is externally mounted. For this option, it would require the use of an appropriate sized additional EZM main lug terminal box within the EZM line up and connect the EMA inside this additional main lug terminal box to the main lugs. The lug sizes in the EZM terminal boxes will accommodate the wires for the EMA. It would be recommended to obtain the EMA reference document 1310CT0202 and the EMA series Instruction bulletin document 8222-0014.

Schneider Electric USA

Attachment(s)
Multi Metering Secondary Surge Protective Device Mounting Kit MMSAMK400 Ser M01.pdf [275.71 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings