Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement meter socket jaw for the MP Meter-Pak or EZM branch devices?

Article available in these languages: Spanish

Issue:
Current Design repair parts

Product Line:
MP and EZM Metering

Resolution:
Replacement meter socket jaws for the residential MP, MPR, MPH, EZM, EZMR, or EZMH devices are as follows:
1) The meter socket jaw assembly is part number 7329794850 (4 jaws are used per 1 phase meter socket; 6 jaws are used per 3 phase meter socket)
2) The meter socket jaw blade guide is part number 4052761901 (1 per meter socket jaw)
3) The keps nut to attach the meter socket jaw is part #2342702001 (1 per meter socket jaw)
4) The meter socket jaw assembly with the blade guide is part number 7329746450 (4 jaws are used per 1 phase meter socket; 6 jaws are used per 3 phase meter socket)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings