Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do we have an NQ panelboard with a 225A main circuit breaker with a 120 Vac shunt trip on the main?
Issue:
NQ panelboard availability, with a 225A main circuit breaker with a 120 Vac shunt trip on the main

Product Line:
Products sold and used in North America

Environment:
NQ panelboards.

Cause:
Selection.

Resolution:
Yes, order the NQ interior needed and main breaker kit NQMB2HJ and order JDL36225SA.  Another option would be to use JDL36225 and field installable shunt trip number S29386.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings