Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Should lugs be ordered separately when ordering a 3 phase individual meter socket, and if so how many?
Issue:
Selection

Product Line:
Individual Meter Socket

Cause:
Selection of lugs

Resolution:
This depends on the catalog number, some come with lugs and some do not. One needs to review a drawing of the specific catalog number to determine if lugs are provided or not. If a socket does not come with factory-installed lugs, first consider the wire size required to ensure proper lug selection, then 3 line and 3 load side phase lugs as well as 1 line and 1 load side neutral lug.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings