Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the wire size for the neutral in a NF430L2C? Or a NFN2CU kit ?
Issue:
What is the conductor capacity for the NFN2CU neutral kit?

Product Line:
NF panelboards and accessories sold and supported in the USA.

Environment:
Installation/specification

Resolution:
The main neutral lug in the interior is for 1 #6-350kcmil and the branch lugs in the interior or kit are for 8- #14-2/0 and 34-#14-#6 AL or CU .
Note that the standard neutral shipped with the NF430L2C is aluminum. However, the replacement neutral, the NFN2CU is available only in copper.
We do not offer a replacement aluminum neutral kit


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings