Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the replacement parts for the H3612AWK, series F6? (may be shown as F06)
Issue:
H3612AWK series F6 repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The replacement parts for the H3612AWK, Series F6 (F06) are as follows. No other parts are available.
Line Base Assembly - 4056603950 (1 required; arc suppressor assembly, fuse puller not included)
Load Base Assembly - 4056604150 (1 required)
Arc Suppressor Assembly - 4056635550 (1 required)
Fuse Puller Kit - FPK0610
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056646950 (recommend replacing switch mechanism gasket)
Switch Mechanism Gasket - 4056603201
Handle Assembly - 4056663550
Handle Gasket - 4056603101
Lockplate - 4056672101
Line & Load base mounting screw - 4020515101 (3 for line and 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)
Equipment Ground Lug Kit - GTK03C

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings