Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between a RFK03 and a RFK03H?
Issue:
Product Features

Product Line:
HD Switch Accessory

Resolution:
The RFK03 rejection clip kit is used with a 9422TC30 operating mechanism for conversion to Class R fuses only. Whereas the RFK03H is for the 60 A, 240 V, series F4-F7 and 30 A, 600 V, series F1 and F5-F7 heavy duty safety switches.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings