Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H366DS, series E2 or E4 heavy duty safety switch?
Issue:
Design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN366AE2 (Obsolete, NLA will need to obtain Line and Load Base Assembly's separately)
Line base assembly - 4055221450SEL (3 required; arc suppressor assembly not included)
Load base assembly - 4055221550SEL (3 required)
Arc suppressor assembly - 4051270850SEL (3 required) Obsolete and replaced by 4051270850
Lug assembly - 4025602450 (2 required per base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (2 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051219150SEL
Vault handle - 4051219450SEL
Handle knob kit - 4401142750
Load Fuse base - 4051212401

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings