Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H366NAWK, Series E2 heavy duty safety switch?
Issue:
Previous Design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN366NAE2 (includes line & load base assemblies, neutral assembly, arc suppressor assembly, box insulator, line phase insulators, and mounting hardware)
Line base assembly - 4055221450SEL (3 required; arc suppressor assembly not included)
Load base assembly - 4055221550SEL (3 required)
Arc suppressor assembly - 4051270850 (3 required)
Lug assembly - 4025602450 (2 required per base assembly)
Neutral assembly - H600SNC
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 405219101 (2 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Vault handle - 4051219450SEL
Handle knob kit - 4401142750
Neutral bonding strap - 4028325350SEL

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings