Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do any of the electrical interlock kits for the safety switches provide form C contacts?
Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Resolution
No, the electrical interlocks used with safety switches provide form Z or ZZ contacts.
The electrical interlock kits with 1A (NO) and 1B (NC) will have form Z contacts and utilize the 9007A01 snap switch to provide the contacts.
The electrical interlock kits with 2A (NO) and 2B (NC) will have form ZZ contacts and utilize the 9007CO3 snap switch to provide the contacts.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings