Issue:
Mini Power Zone Transformers have a standard temperature rise of 115C
Product Line:
LV Transformers
Environment:
Applies to Mini Power Zone Transformers from SquareD/Schneider Electric
Cause:
Mini Power Zone Transformers can be ordered with an 80 Degree C Temperature Rise
Resolution:
Yes, up to 15KVA , single , or three phase MPZ Transformers can be quoted with 80 Deg C temperature rise
Mini Power Zone Transformers have a standard temperature rise of 115C
Product Line:
LV Transformers
Environment:
Applies to Mini Power Zone Transformers from SquareD/Schneider Electric
Cause:
Mini Power Zone Transformers can be ordered with an 80 Degree C Temperature Rise
Resolution:
Yes, up to 15KVA , single , or three phase MPZ Transformers can be quoted with 80 Deg C temperature rise
Released for: Schneider Electric USA