Issue:
Why are there are two different length of wire binding screws in the AL600LS52K3 kit?
Product Line:
Powerpact L frame breakers
Resolution:
AL600LS52K3 has a wire range of 2/0 to 500 KCMIL. The longer screws are factory installed on the lugs and the shorter ones are shipped in the kit. The shorter ones are used for larger wire to prevent interference with the lug shield.
Why are there are two different length of wire binding screws in the AL600LS52K3 kit?
Product Line:
Powerpact L frame breakers
Resolution:
AL600LS52K3 has a wire range of 2/0 to 500 KCMIL. The longer screws are factory installed on the lugs and the shorter ones are shipped in the kit. The shorter ones are used for larger wire to prevent interference with the lug shield.
Released for: Schneider Electric USA