Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do ALL the EZM Main Devices(Terminal box, Circuit Breaker, fusible switches) come standard with a neutral bonding strap?
Issue:
Product Design Features

Product Line:
EZ Metering equipment

Environment:
Neutral Bonding Strap

Cause:
Application

Resolution
Yes, but there are a couple exceptions(see below), so ALL the EZM Main Devices will come standard, from the factory, with a neutral bonding strap.

EXCEPTIONS: The EZM1225TB and EZM3225TB are ONLY supplied with an isolated neutral and cannot be bonded. They are NOT Suitable for use on the LINE side of Service Equipment.

NOTE: SEE EACH CATALOG NUMBER REPAIR PARTS FAQ FOR THE BONDING STRAP PART NUMBER.



Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings