Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU664AWK, series F6? (may be shown as F06)
Issue:
Repair parts list for HU664AWK, series F6

Product Line:
Safety Switches

Resolution:
The repair parts for the HU664AWK, series F6 (F06) are as follows. No other parts are available.
  • Complete Line/Load Base (all one piece) - 4056704351 (includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
  • Line/Load Base mounting screws - 4020506501 (12 required per line base)
  • Arc Suppressor Assembly - 4056677550 (1 required)
  • Arc Suppressor mounting screw - 4020514501
  • Lug Assembly - 4025136550 (per lug)
  • Lug Assembly mounting screw - 2140122240
  • Switch Mechanism - 4056740150 (requires interlock shaft gasket 4056786001)
  • Switch Mechanism mounting screws - 2299940562 (2 required)
  • Handle Assembly - 4056746850 (requires handle gasket 4056603101)
  • Lockplate - 4056746701
  • Lockplate mounting screws - 2299940562 (2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings