Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H363RB, series F5? (may be shown as F05)
Issue:
Repair parts

Product Line:
Safety Switches

Resolution:
The replacement parts for the H363RB, series F5 (F05) are as follows. No other parts are available.
  • Interior kit - HSIF310F (includes line and load base assemblies, mechanism, arc suppressor, all mounting hardware, and instructions)
  • Line Base Assembly - 4056775150 (1 required)
  • Line Base mounting screws - 4020515101 (3 required)
  • Load base kit - HLB310F (includes load base and mounting hardware).
  • Load Base Assembly - 4056602850 (1 required)
  • Load Base mounting screws - 4020515101 (2 required)
  • Lug kit - AL10F (includes 6 lugs and mounting screws)
  • Arc Suppressor kit - HAS0610F (includes arc suppressor and mounting hardware)
  • Arc Suppressor assembly - 4056635550 (1 required)
  • Arc Suppressor mounting screws - 4020514501 (1 required)
  • Handle/Mechanism kit - HM0610F (includes handle, mechanism, lockplate, and mounting hardware)
  • Handle Assembly - 4056663550 (operating handle only; requires handle gasket)
  • Handle Gasket - 4056603101 (1 required with the replacement of the handle assembly)
  • Lock Plate - 4056672101 (1 required)
  • Lock Plate Mounting Screws - 2299940562 (2 required)
  • Mechanism Assembly - 4056646950 (1 required and requires the interlock gasket)
  • Mechanism Interlock Gasket - 4056603201 (1 required with the replacement of the mechanism assembly)
  • Cover Latch - 4056607201 (1 required)
  • Cover Latch Spring - 4022304301 (1 required)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings