Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there an End Tap box termination option for AP50610 I Line Busway?
Issue:
Is there an End Tap box available to terminate to an AP50610 piece of  I Line Busway?

Product Line:
I Line Busway

Environment:
Plug in tap box for 600 amps only choice, which takes up plug in slot in Busway

Cause:
Factory option for custom End tap box needed

Resolution:
AP50612ETBS ( for a run that ends with a bolt) or an AP50612ETBB ( for a run that ends with a slot) . Price is available using per foot pricing in the Digest, plus adding the tap box fitting charge.











Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings