Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H365AWK, Series E5 (E05) heavy duty safety switch?
Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4055218850 (3 required; arc suppressor assembly not included)
Load base assembly - 4055219050SEL (3 required)
Arc suppressor assembly - 4051270850 (3 required)
Lug Assembly - 4025113650 (1 required per base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217251
Handle knob kit - 4028343550
Cover opening Thumb Screws - 4405043401 (2 required)
Thumb Screws retainer - 4405043301 (2 required)
Cross Bar Insulator - 4055217701 (2 required)
Cross Bar Insulator - 4055217801(1 required)
Cross Bar Insulator - 4055227601(1 required)
Dust Shield - 4055215701 (1 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings