Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an HU365DS, Series E5(or E05) heavy duty safety switch?
Issue:
Current Design Repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4055218950SEL (3 required; arc suppressor assembly not included)
Arc suppressor assembly - 4051270850 (3 required)
Line base lug assembly - 4025113650 (2 required per line base assembly)
Line base lug mounting screw - 2140128481 (1 per lug)
Line base lug mounting nut - 2342702800 (1 per lug)
Line base phase insulator - 4055219301 (2 required)
Line base mounting screws - 4020600901 (2 required per line base assembly)
Handle assembly - 4051219151
Handle knob kit - 4028343550
Right cross bar insulator - 4055217701( 2 required)
Middle cross bar insulator - 4055217801 (1 required)
Left cross bar insulator - 4055227601 (1 required)
Dust Shield - 4055215701 (1 required)
Door thumb screws - S1A99898 (2 required)
Door thumb screw retainers - 4405043301 (2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings