Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a 20 amp or 30 amp EH or EHB breaker be installed opposite an EHB34100 ?
Issue:
Installing a 20 amp or 30 amp EH or EHB Bolt on breaker opposite an EHB34100

Product Line:
NEHB Panlboard

Environment:
Installation

Cause:
Clarification

Resolution:
No . You can not place any breaker across from 70-100A  EHB breakers.  They have a rejection feature which prevents it and that is due to heat issues.
The NEHB panel and Eh/EHB breakers are obsolete and no longer supplied by Square D /Schnedier Electric. The NF Panelboard with ED/EDB breakers, are currently offered

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings