Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does the HL100WN2M16 come with the steel roller lever arm?
No the steel roller lever arm must be purchased separately.   The body is machined aluminum, the roller itself is steel.
We offer different lengths like the 1.50  inches would be part number AA.

2.00 is AH
2.50 is AO
2.75 is AK
3.00 is AB
4.00 is AM
6.00 is AR


CTA-ID : 2062391

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings