Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the 9036FG30 contacts open on liquid rise?
Issue:
Can the 9036FG30 contacts open on liquid rise?

Product Line:
Float switches

Environment:
9036FG

Cause
operation, modification, and features

Resolution
9036FG30 can be field converted from NC to NO.  The switch plate and mounting base have holes for the float rod on both ends. Installing the rod on the high end of the switch plate when the contacts are closed allows the device to empty a sump. Installing the rod on the high end of the switch plate when the contacts are opened allows the the device to fill a tank.

Schneider Electric USA

Attachment(s)
9049A6.pdf [126.68 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings