Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H365DS, series E4 heavy duty safety switch?
Issue:
Repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
Answer The parts listed here are the only field replaceable parts.
Line base assembly - 4055218850 (3 required; arc suppressor assembly not included)
Load base assembly - 4055219050 (3 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Arc suppressor assembly - 4051270850 (3 required)
Line/Load Main Lug Assembly - 4025113650 (1 required per line or load base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (1 required)
Handle assembly - 4051219151 (may require 2 mounting screws 2140122242 and washers 2370100220)
Vault handle - 4051219450SEL
Handle knob kit - 4028343550

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings