Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can compression lugs be used on Powerpact P frame and R frame I-Line breakers?

Issue:
Can compression lugs be used on Powerpact P frame and R frame I-Line breakers?

Product Line:
Powerpact P frame and R frame circuit breakers

Resolution:
Yes, they can be used, but in panelboards, they require use of an end gutter box extension.
Compression lugs extend beyond the load end of a circuit breaker and an end gutter or side gutter box extension is required to meet electrical code wire bending requirements.
When a factory assembled panelboard with compression lugs is specified in Quote to Cash, the Panelboard Product Selector will automatically configure the necessary box extension(s).
I-Line panelboards are cULus listed with mechanical or compression lugs.
See product data bulletin 2110DB0901 .

Schneider Electric USA

Attachment(s)
Compression Lugs I-Line 2110DB0901.pdf [1.17 MB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings