Issue:
The DJM32400E20 tenant circuit breaker in a 400A EZML or EZMK, Series M02, needs to be replaced.
Product Line:
Metering Equipment.
Environment:
EZ Metering Devices.
Resolution:
The DJM32400E20 can be replaced with the LJM36400U31X. When the EZML branch is a single phase device, the B phase (center) lug should be removed from the ON end of the breaker.
Released for: Schneider Electric USA