Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Why does Binary Value Objects Instance #4 HAND/AUTO ACT not change state when the AFC/OFF/BYPASS switch is changed on the S-flex system?

Issue:
Controlling the ATV212 with BacNet shows hand control when its in auto mode.

Product Line:
SFD212 series S-flex

Environment:
All ATV212 S-flex systems equipped with Bacnet for monitoring AND/OR Control.

Cause:
Misuse of BVOI#4

Resolution:
Binary Value Objects Instance #4 will change state to indicate if the drive is in local or remote mode.  This BVOI changes when the LOC REM button on the face of the drive is pressed to indicate if the drive is being controlled remotely, or locally from the built-in keypad on the drive.   It will not change state with the HAND/OFF/BYPASS  switch on the front of the S-flex cabinet.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings