Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a field conversion option for 8536SE to change the overload relay to accept slow trip SB (slow Blow) and FB (quick trip) thermal units?
Issue
What is needed for an overload relay size 3 to accept slow trip and quick trip thermal units?

Product Line
NEMA and Definite Purpose Contactors and Starters

Environment
Type S Starters and overloads

Cause
modification, retrofit

Resolution
The standard melting alloy overload relay will have to be replaced with the special modified block in order to install the Slow trip and quick trip thermal units. For a replacement 8536SE NEMA size 3 three pole overload order the 9065SDO12Y81.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings