Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: Do Sealed Resin Epoxy Encapsulated Transformers need lug kits or do they have screw type terminals?
Issue:
Do the Sealed Resin Epoxy Encapsulated Transformers require accessory lugs or terminals?

Product Line:
LV Transformers

Environment:
Applies to Sealed Resin Epoxy Encapsulated Transformers ONLY

Cause:
Sealed Resin Epoxy Encapsulated Transformers use a different wiring method than Ventilated or Non Ventilated or Control Transformers

Resolution:





Sealed Resin Epoxy Encapsulated Transformers are typically mounted on a wall or vertical surface and wired at the bottom. No lugs or screw terminals are required. Wiring is done by means of wire nuts, or split bolts and tape. The Primary and Secondary connections are flexible wires in the wiring compartment of the enclosure. The wires can be connected to the source and load, and are then pushed back up into the enclosure wiring compartment, and the bottom covers replaced.

The photo below shows an un mounted Sealed Resin Epoxy Encapsulated Transformer placed upside-down on a flat surface with one wiring cover removed. Note the available knockouts on the lower section of the enclosure on the front, back, sides, and bottom for conduit entry.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings