Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How is the current rating on an ATS48 soft start determined from the part number?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

The ATS48 part numbering system is as follows:

The letter after ATS48 indicates the placement of the decimal point with the following 2 digits.
"D" means there are 2 digits to the left of the Decimal:  (Example:  ATS48D17Y would be rated for 17.0 amps)
"C" means there are 3 digits to the left of the decimal:  (Example: ATS48C17Y would be rated for 170.0 amps)
"M" means there are 4 digits to the left of the decimal: (Example:  ATS48M12Y would be rated for 1200.0 amps)


ATS48 softstart current ratings:
ATS48D17Y - 17A          ATS48C11Y - 110A          ATS48M10Y - 1000A
ATS48D22Y - 22A          ATS48C14Y - 140A          ATS48M12Y - 1200A
ATS48D32Y - 32A          ATS48C17Y - 170A
ATS48D38Y - 38A          ATS48C21Y - 210A
ATS48D47Y - 47A          ATS48C25Y - 250A
ATS48D62Y - 62A          ATS48C32Y - 320A
ATS48D75Y - 75A          ATS48C41Y - 410A
ATS48D88Y - 88A          ATS48C48Y - 480A
ATS48C59Y - 590A
ATS48C66Y - 660A
ATS48C79Y - 790A

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings