Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a GFM150HD or GFM250JD be operated on a 3w system without a neutral, and how is it wired?
Issue:
Using Ground Fault Module

Product Line:
Ground Fault Equipment

Resolution:
Yes, it can be operated on a 3w system, provided the system is grounded.

On this system, the neutral CT is not required, therefore leave terminals 5 and 6 open. Do not jumper terminals 5 and 6.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings