Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What can be used to replace an old Isolation Monitor 43134-007-50 or IGD line isolation monitor ?

Article available in these languages: Spanish

Issue:
Replacing an IGD line isolation monitor or an old Isolation Monitor 43134-007-50

Product Line:
Medical Products

Environment:
LIM

Cause:
Not functioning

Resolution:
There generally is a remote indicator/annunciator associated with a LIM . (This "remote" can be located on the isolation panel with the LIM or be installed on a wall.) Please see below for options:

1. If either a ORICA or IA1C is in use, replace the IGD with an IG6M, a 4800IG6CBKTVM (connector plate and mounting bracket kit)and a 4800XMIA transformer ( or get a complete IG6ADKIT).

2. If the remote is an RA1* model, use an IG6M, a 4800IG6CBKTVM (connector plate and mounting bracket kit)and a 4800RA1WMAHA converter box with wiring harness( or get a complete IG6DDKIT).

3. If there is no indicator, use an IG6M with a 4800IG6CBKTVM (connector plate and mounting bracket kit)

Please review the attachment for more information and specifics for other accessory replacements.

Schneider Electric USA

Attachment(s)
4805CT1301 IG6M catalog and replacements.pdf [3.01 MB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings