Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
The IG6M line isolation monitor (LIM) has an information message 8.8.
Issue:
Information Message "8.8" on the IG6M Isolation Monitor. What does this mean and how does one correct it?

Product Line:
Hospital Isolated Power Systems

Environment:
NFPA99, NEC517.160

Cause:
Commissioning, reset

Resolution:
The information message 8.8 indicates the date and time stamp must be reset.  Resetting the LIM clock will remove the information message. Please refer to attached document, or the IG6M LIM Manual MED10110103 for menu structure.

Schneider Electric USA

Attachment(s)
IG6 SET_UP_ERROR8.80_2-12.pdf [278.33 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings