Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the fingersafe cover for an FAL/FHL circuit breaker?
Issue:
Circuit breaker fingersafe covers.

Product Line:
FAL/FHL Circuit Breakers

Environment:
Safety

Cause:
Query

Resolution:
The fingersafe cover is part number FCA1A.  It comes two per kit, one for the load side and one for the line side.
FAL/FHL breakers are obsolete and no longer available.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings