Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
When is isolated power required?
Issue:
Isolated Power, when is it needed?

Product Line:
Hospital Isolated Power Systems

Environment:
NFPA99, NEC517.160

Cause:
Codes and Standards

Resolution:
In wet procedure locations in hospitals, special protection against electrical shock is required, and this is attainable by using Class A GFCI or an isolated power system. For electrical safety, the NEC recommends isolated power systems, which should be installed whenever a power outage cannot be tolerated during a ground fault condition.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings