Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the phenolic strips with horizontal permanent numbers for the NQ 42 and 84 circuit panels ?

Issue:
Part number for the permanent number strips for the NQ panels

Product Line:
Panelboards

Environment:
NQ

Cause:
Labelling

Resolution:
80110-190-09 is for the  strip numbered 1-41 .80110-190-10 is for strip numbered 2-42. These 1/4"w strips have black letters on white background and are mounted vertically on the deadfront . Two screws are provided. Number strips for 43-84 horizontal would be (2)80110-192-05SPL engraved as 43-83 and 44-84 ODD.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings