Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does the "NF" mean on the end of this # .....MH50WPSSULNF?
Issue:
MH Stainless Enclosure

Product Line:
Panelboards

Environment:
NF and NQ

Cause:
Clarifying catalog number

Resolution:
It means the box has the trim/gutter cover kit that fits the NF deadfront width. When NQ was created the NQ deadfront became the same width as the NF so the N3R & 4X gutter covers became the same for either panel. Before NF there was both a NQ and NF version of gutter covers. Now we only need the "NF" version since the NQ deadfront became the same profile as the NF. It is confusing when folks see the NF.

Schneider Electric USA

Attachment(s)
MHWPSSUL.pdf [44.73 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings