Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the recommended number of conductors and conduit size for 120V branch circuits in a hospital isolated power system?
Issue:
Recommended number of conductors and conduit size for 120V branch circuits in a hospital isolated power system

Product Line:
Hospital Isolated Power Systems

Environment:
NFPA99, NEC517.160

Cause:
It is necessary to complete the installation of a hospital isolated power system in a manner which will comply with special requirements and pass required testing and certification.

Resolution:
3/4" conduit is recommended with no more than 6 conductors per conduit to help minimize leakage.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings