Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a surge protective device (formerly TVSS) be installed on an isolated power system?
Issue:
Application

Product Line:
Install TSS device on a Hospital Isolated Power System

Environment:
NFPA 99, NEC 517.160

Cause:
Installation / Setup

Resolution:
No, these devices are designed for grounded systems and should not be installed in Isolated Power Systems. UPS/surge protective devices normally include inverters, suppressors and filters which compromise the proper function of the Line Isolation Monitor.

Schneider Electric USA
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings