Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the filler plate for the EDB, EGB, and EJB breakers, used in pre-series E1, NF panelboards?

Article available in these languages: Spanish

Issue:
Filler plate for the EDB, EGB and EJB breakers, used in pre-Series E1 NF panelboards

Product LIne:
PTFDS - FD Enclosure Systems NF Panelboards

Environment:
NF circuit breaker panelboards sold and supported in North America

Cause:
Correct replacement filler plate contingent on panelboard series.

Resolution:
EFP is the single pole filler plate. This filler plate should not used in the current style E1, only on Series 0 panelboards built prior to October, 2008.
NFFP15 is the single pole filler plate to be used on Series E1 NF panelboards built after October , 2008.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings